4/6/2016 5:09 PM | |
Joined: 5/28/2008 Last visit: 8/6/2024 Posts: 4515 Rating: (838)
|
Hello, This cable as far as I remember doesn't come with a driver. It should be installed if you have recent version of MICROWIN or even WinCC flexible. This cable is used for download or upload of S7-200 PLCs and also some SIMATIC Panels. In any case, there may be some difficulties with some old versions CPU. Please revise the info in the following FAQ. It stated clearly that for these old CPUs you should use serial PPI cable! Why do you get an error message when program downloading in various S7-S7-21x CPUs via USB/PPI or RS-232/ PPI Multi Master cable?In any case, please tell us what type and part number of PLC or SIMATIC Panel you would like to use the PPI cable with. Hope this helps. |
Ayman Elotaify |
|
This contribution was helpful to1 thankful Users |
4/6/2016 7:43 PM | |
Joined: 9/27/2006 Last visit: 8/14/2024 Posts: 12277 Rating: (2680) |
Hello ViciTech; If you plan to run Microwin 4.0 under Win 7 (32- or 64-bit), you should install SP9.
STEP7 MicroWIN V4.0 SP8 and SP9
https://support.industry.siemens.com/cs/ww/en/view/58523240
See the attached screenshot. Hope this helps, Daniel Chartier |
This contribution was helpful to4 thankful Users |
4/13/2016 12:37 PM | |
Posts: 4 Rating: (0) |
Hi!! Thanks very much!! Regards, |
This contribution was helpful to2 thankful Users |
11/25/2016 12:55 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by luias is split to a separate thread with the subject PC / PPI cable driver. Best regards |
Follow us on