4/13/2016 9:06 PM | |
Joined: 3/14/2008 Last visit: 9/13/2024 Posts: 2095 Rating: (936) |
Hi Rozen, If you want to use multiple operator stations based on the same configuration, Siemens recommends using a Reference OS. A reference OS makes use of another OS (base OS). You will configure the base OS only. This means that for one single station, you have to insert not a "WinCC Application", but a "WinCC Application Ref". On that reference OS, you have to set which is the base OS by going to the reference OS->Edit->Object Properties->OS Ref->Options for OS reference objects. Select the base OS from the dropdown menu and then enter the path for the reference OS. Edit: Please make sure that both single stations are within one project in the multiproject. |
Last edited by: Oreca at: 4/13/2016 9:07:39 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/14/2016 10:59 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by Rozen is split to a separate thread with the subject Connect os reference to AS directly with cp1623. Best regards |
Follow us on