4/17/2016 10:24 PM | |
Posts: 4 Rating: (0) |
And i'm also interested for communication two,or three 0ba8 through LAD. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/18/2016 10:34:45 AMNew subject after splitting |
|
4/17/2016 10:37 PM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191) |
Unfortunately (or thank goodness) network projects are supported only in FBD. |
4/18/2016 12:02 AM | |
Joined: 12/18/2014 Last visit: 9/12/2024 Posts: 33757 Rating: (4191) |
Here is a small example of the communication between two 0BA8 in LAD.
Attachment0BA8_Server_Client.zip (239 Downloads) |
This contribution was helpful to2 thankful Users |
4/26/2016 9:22 PM | |
Posts: 4 Rating: (0) |
I finally got three 0BA8,and have some fun with three pieces of communication in the LAD. If some help,here is the result. Greetings from Croatia I recorded the video,so here... Attachment0BA8_3pieces_Server-Client.zip (217 Downloads) |
Last edited by: Hlapic at: 4/27/2016 8:50:31 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on