4/22/2016 2:31 AM | |
Posts: 9 Rating: (0) |
Hi, I need connect PLC 6ES7214-1BG40-0XB0( V4.1.1), but to connect sends me an error message "not compatible". I have TIA V13 Sp1 Up 8.... |
4/22/2016 5:27 AM | |
Posts: 153 Rating: (9) |
Do you chooose right PLC number, right firrmware |
This contribution was helpful to1 thankful Users |
4/22/2016 7:13 AM | |
Posts: 9 Rating: (0) |
I can watch the program but, I cant download the blocks to edit. Only can choose v4.1 and the plc have V4.1.1...That may be the problem? |
4/22/2016 8:30 AM | |
Joined: 4/24/2006 Last visit: 7/12/2024 Posts: 8711 Rating: (1166) |
Hello, Perhaps this link might help: Best regards, Wizard |
4/22/2016 8:45 AM | |
Posts: 9 Rating: (0) |
CALL ME TO THE CALL CENTER OF MY COUNTRY AND I TOLD MY TIA V13 UPGRADE NEEDED FOR THE CPU HAS FIRMWARE v4.1.3. SOMEONE KNOWS HOW TO DO THAT? |
Follow us on