(2)| 4/27/2016 6:42 PM | |
|
Posts: 5 Rating:
|
I have not siemens encoder OIH-48-2500P8-L6-5V http://www.tamagawa-seiki.com/pdf/download/1228N55EJ_shusei.pdf pages 25-26 Oscilloscope view in attach. There is a little noise, but it does not interfere with work. The maximum frequency that I can set on axis is 30 kHz I made series of mistakes: 1. I use single channel from encoder 2. I use DWOD type When the encoder was connected through two channels, the maximum frequency of the resulting halt of about 65535 Hz. This corresponding to two bytes. Using REAL, UDINT (4 bytes) type of %ID1000 doesn't help. Any ideas? |
Follow us on