4/27/2016 7:52 AM | |
Posts: 200 Rating: (6) |
can u program the S300 plc from this software or is it just the ones listed in the plc list that are the 1200s |
4/27/2016 7:56 AM | |
Joined: 12/4/2009 Last visit: 5/3/2024 Posts: 452 Rating: (135) |
Andrewdaw, it is possible to program S7300 in TIA portal, you only have to be careful with the firmware version - only some CPU's support this feature. You may also want to check TIA Portal Readiness Check. Hope this helps. Regards. |
Last edited by: crazyCow at: 4/27/2016 7:58:52 AMIf this post actually helped, you may consider using the Rate button above. |
|
This contribution was helpful to1 thankful Users |
4/27/2016 7:58 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
In the link bellow you can find info about. |
Last edited by: UMENCHO at: 4/27/2016 7:59:16 AM |
|
4/27/2016 2:38 PM | |
Joined: 8/21/2014 Last visit: 5/23/2024 Posts: 962 Rating: (13) |
New question published by Arasan is split to a separate thread with the subject Updating from WinCC Basic to Professional?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on