4/30/2016 7:31 AM | |
Joined: 11/21/2007 Last visit: 7/7/2024 Posts: 2325 Rating:
|
Hello In SIMATIC STEP 7 V5.5 and other SIMATIC software products released for Windows 7, the required driver for the SIMATIC USB Prommer and the PC Adapter USB are part of SIMATIC Device Drivers. A separate installation of the drivers as before via the CD supplied together with the PC Adapter resp. USB Prommer is thus no longer necessary. Please check the Settings in the PG PC interface and the connection with PLC. |
Last edited by: Navnag at: 4/30/2016 7:35:34 AMThere is no such thing as the last bug in a program |
|
This contribution was helpful to
1 thankful Users |
4/30/2016 7:54 AM | |
Joined: 3/28/2015 Last visit: 6/17/2024 Posts: 721 Rating:
|
Hello, Kindly find the attached file. AttachmentS7_Downloading_ Uploading.pdf (1019 Downloads) |
Eng.Mohamed Ibrahim |
|
5/1/2016 8:50 AM | |
Joined: 3/17/2013 Last visit: 7/15/2024 Posts: 481 Rating:
|
Also take care that you are connecting on CPU to MPI port. Regards, Vijay |
Follow us on