5/1/2016 2:38 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Perhaps the following topics might help: |
Eng.Mohamed Ibrahim |
|
5/1/2016 5:25 PM | |
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, For the two mentioned Panel, You can do the factory rest using one of the following cables / connectors:
Third cable can be made using cheap materials (just buy Sub-D 9 pin sockets and cable and connect it 1:1) It should work. The Reset to Factory setting is available only for the above mentioned cables in according to the excel sheet attached to entry ID: 19109408 You have to search for cables with character "U" Hope this helps. |
Ayman Elotaify |
|
8/31/2016 11:33 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by a2kon2 is split to a separate thread with the subject KTP600 lost his program during load shedding. Best regards |
Follow us on