(0)| 5/17/2016 2:45 AM | |
|
Posts: 3 Rating:
|
I hate to bring an old thread back from the dead but I am in a similar situation but the "system constants - Hw_Interface" data types seem to be read-only. How can I change the HW_Interface type in the System Constants area? I'm using TIA V13 SP1 Upd 8, and I read somewhere else that I could modify the name of the device/port and that it would in turn modify the index of the hardware. ------------------------------------------------------------------------------------------ |
Last edited by: MattyManny at: 5/17/2016 2:46:39 AMLast edited by: Min_Moderator at: 5/17/2016 11:57:50 AMNew subject after splitting |
|
Follow us on