5/22/2016 1:38 PM | |
Posts: 1 Rating:
|
Hello how I can make a program that allows the user to enter two variable "longueure: x" and "quantity: y" with the TD 200 v2.1 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 5/23/2016 10:44:03 AMNew subject after splitting |
|
5/22/2016 2:17 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating:
|
Hello eltamed; First, what CPU model number and version of MicroWin do you use in your project? In the 9relatively) newer versions there is a TD 200 configuration Wizard in MicroWin that simplified the task of creating the parameter bolock for the TD 200. The online hwlp will guide you to the use of the wizard, if your version of MicroWin supports it. If you do not have this wizard, you can still easily define the parameters for data exchange between the CPU 200 and the TD 200, with a bit more work. Here are a few information sources: Configuring the TD200 https://support.industry.siemens.com/cs/ww/en/view/459430 Various FAQs on the TD200: https://support.industry.siemens.com/cs/search?search=program%20TD200&type=Faq&lc=en-WW Video Tutorials for the S7-200: Demonstration System: SIMATIC S7-200 Video Tutorials (see the video on Text Displays) https://support.industry.siemens.com/cs/ww/en/view/30839030 and of course the manuals: TD 200 Operator Interface (TD 200 Version 1) (OLDER models) https://support.industry.siemens.com/cs/ww/en/view/14946222 S7-200 SIMATIC Text Display (TD) User Manual (NEWER models) https://support.industry.siemens.com/cs/ww/en/view/1087140 S7-200 System manual https://support.industry.siemens.com/cs/ww/en/view/1109582 Hope this helps, Daniel Chartier |
This contribution was helpful to
2 thankful Users |
Follow us on