5/24/2016 9:24 AM | |
Posts: 124 Rating:
|
Hi, Attached a Project for a LAN (Local Area Network), merely as an example. Suppose I have two Logo 8, where each one has its program and its message text. Each Logo will work with an exclusive TDE. Based in a have read, I can say: 1. To link TDE_1 to Logo_1 I have to click in Logo_1 in <Project View>, select <Add Server connection>, mark the check box <Connect to Operator Panel>, type IP address of the TDE_1 yet added and the same TSAP for the Logo_1. The message of circuit program Logo_1 will be showed in TDE_1. 2. I have to proceed the same to Logo_2. Am I right? In time: suppose that the devices address was changed according the LAN. Tanks in advance. AttachmentProject in doubt 2.zip (395 Downloads) |
5/25/2016 5:26 AM | |
Joined: 12/18/2014 Last visit: 7/5/2024 Posts: 33296 Rating:
|
I'm sorry, but I do not understand you. For communication between Logo and TDE there must no connection be created. Look at attachment. AttachmentLOGO! 8 Soft manual 0BA8 2014_06 sides 329-336.pdf (706 Downloads) |
This contribution was helpful to
4 thankful Users |
Follow us on