6/6/2016 7:18 PM | |
Posts: 8 Rating: (0) |
hi . i have a 6sn1118-0aa11-0aa0 controller for driving a servo motor . i have a problem . My drive status is Ok but i can't run it . when i connect Terminal 65 , 9 (Controller enable) without ref , my output current increase suddenly until drive trip and motor warm up . what must i do ? how i should adjust 4 potensiometers on drive ???? PLease help me . i will add some photos. with best regards ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/7/2016 9:01:32 AMNew subject after splitting |
|
6/7/2016 9:49 AM | |
Joined: 4/23/2010 Last visit: 11/14/2024 Posts: 8092 Rating: (878) |
Is this problem of running machine or installation/commissioning of new drive? Please read download & refer below manual for detailed information. SIMODRIVE 611 analog, Transistor PWM Inverters for AC Feed Drives and AC Main Spindle Drives |
Follow us on