6/8/2016 8:49 AM | |
Joined: 11/8/2014 Last visit: 1/9/2022 Posts: 7 Rating: (0) |
Hello everyone, its possible recursivity in Siemens 1200?? Estoy tratando de conseguir una función recursiva y no me la reconoce... ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 6/8/2016 9:17:38 AMNew subject after splitting |
|
6/8/2016 9:19 AM | |
Joined: 8/21/2014 Last visit: 5/13/2024 Posts: 954 Rating: (13) |
Hello EusebioRoncal,
this is an English speaking forum. Thus please write in English only. Thanks.
Best regards The Helping Hand |
My Forum is the place to personalize your profile, |
|
This contribution was helpful to1 thankful Users |
6/8/2016 4:01 PM | |
Joined: 7/7/2010 Last visit: 5/13/2024 Posts: 14710 Rating: (2359)
|
This is a deterministic system be design, and recursive calls may not necessarily complete in a specified amount of time and as such are strongly discouraged. Many PLC manufacturers during project compilation will fail if any attempt at calling a routine recursively, or mocking up a method that in the end does the same thing. It is really to protect you from yourself. Instead, think of a way to perform one calculation of the recursion per PLC scan to get a predictable process. Yes, it will take longer to complete the call, but your process will enjoy a more consistent scan time, which usually means things work more smoothly.
|
science guy |
|
Follow us on