10/20/2015 6:11 PM | |
Posts: 13 Rating: (3) |
You can use SFC51 for this. 1) For SF set SSL-ID = W#16#0692 Please check this FAQ. "The status of the DP slave with Address 1 is in Bit 0 of the first byte. If this bit is set, then that DP slave is either defective or disabled. " 2) For BF set SSL-ID = W#16#0292 Please not that these value are valid only if you are using integrated CPU interface. For external DP interface values are W#16#4692 and W#16#4292. For more information you can check the help for sfc51 in your Step 7 installation. |
This contribution was helpful to1 thankful Users |
6/17/2016 10:38 AM | |
Joined: 8/21/2014 Last visit: 8/30/2024 Posts: 1006 Rating: (13) |
New question published by Akshita Saraswat is split to a separate thread with the subject Getting the ACT LED status. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on