6/17/2016 2:53 PM | |
Joined: 5/9/2015 Last visit: 4/9/2024 Posts: 5 Rating: (0) |
i have using the multiple integer value how can find the which integer value max or min in TIA V13 ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/20/2016 1:02:36 PMNew subject after splitting |
|
6/20/2016 4:09 PM | |
Posts: 5225 Rating: (1188)
|
Hi. You are not very specific on which data types, how the data is structured and which PLC is used. That can influence the accuracy of the supplied answer. I think the following links will be helpful when working with S7-1200 / S7-1500.. (1) Library of general functions for STEP 7 (TIA Portal) and S7-1200 / S7-1500 (2) Library with program examples for TIA Portal instructions -- The codes shown in (2), has been developed as general example to each instruction available. It is not yet fully complete, but the MIN and MAX commands are included for your case. |
Follow us on