6/25/2016 12:16 PM |
|
Posts: 92 Rating:
|
Hi there im working on a 810T GA3 and step 5V7.2 on Windows XP in PC Sinumerik 810T ,im also online and my cpu type is :150U my Backups file all is as a ".txt" f.e : PCP.txt PCA.txt TA1.txt and ... and i just can transmit BLOCKS what can i do,convert text files? how? thank to your attention ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/27/2016 3:30:28 PMNew subject after splitting |
|
6/27/2016 3:38 AM | |
Joined: 10/17/2007 Last visit: 8/28/2024 Posts: 4011 Rating:
|
You said you just transmit "blocks" what is blocks mean? --I think you have PCIN or Winpcin SW. so check the file I attached to transfer all back up you have--including PCP and PCA. you don't need STEP 5.
Attachment810_820 reload.pdf (423 Downloads) |
If you like my comments please |
|
6/28/2016 8:02 AM |
|
Posts: 92 Rating:
|
I just explain my Problem in this pdf file . I did not work with step 5 before , so I even dont know how to use "normal rs232 interface." Dear Mr Pee and Dear Mr nulizhang I also insert some picture, with blocks . AttachmentTransfer PC to 810T GA3.pdf (461 Downloads) |
6/29/2016 8:14 AM | |
Joined: 1/30/2007 Last visit: 6/3/2022 Posts: 262 Rating:
|
Hi Sky Diver840, Your topic has been split to this: Please find my response in that topic ... Good luck |
7/5/2016 4:10 AM | |
Joined: 10/17/2007 Last visit: 8/28/2024 Posts: 4011 Rating:
|
1st of all Don't mix things together. PCIN can transfer PLC program in ASIIC code--which you cannot read/ or understand meaning but STEP 5 can transfer S5 code the name like My810T@@.S5D, which you can read by STEP 5 in the format of Ladder or STL, I think you may not have PLC program backup by S5 code, you have PCP.txt for sure but that cannot convert to S5 code, --from you pic's I see you have some FB,'s and DB's , which you said you can transfer . But that is not your m/c real PLC program, they are PLC system blocks stored in EPROM, which YOU NO NEED TO BACK UP OR TRANSFER. Now I give you suggestion for your PCIN TRANSFER REF this link answered by me (your 810TGA3, His 840D with PCU20--your PCIN, his WinPCIN) the guy had similar issue (not same) with you, I think is cable problem. Do you make cable by your self? you made it simple 3 wires TX,RX, GND? I see your display alarm --it seems your cable has no hardware hand shake. so buffer is full --when there is RS232 error, DIO will disappear and transfer will be stopped. I suggest you make better cable --I attached drawing 9-9 pins in that answer, that is easy to Google RS232 cable pinout 25 D to 25 D. making cable at least 5 wires followed drawing. another solution is reduce Baud rate to 600 or 300 ( I don't like this ) PS: I see your pic's the setting data 5011=11000111---that is for 9600 baud rate. I don't know why you said 1200? try as I suggest if you fix it please rate my answer, if not fix, post problem again or you can send PM to me.
|
If you like my comments please |
|
This contribution was helpful to
1 thankful Users |
7/5/2016 10:33 AM | |
Posts: 92 Rating:
|
Dear nulizhang yeah,you right ,we do not have the S5 code for the PLC backup, therefore we believe that if convert the PCIN backup codes to Step 5 codes, we would be able to transfer the backup files to the system. Or do you believe there are any other possible ways to transfer the.txt files on step 5. there is a way ,told me somebody ,who did that before and had the same, problem. thanks so much Regards p.m: is it possible to you check my %PCP and check it to its OK , Please AttachmentPCP.txt (384 Downloads) |
Follow us on