6/27/2016 6:18 PM | |
Posts: 6 Rating:
|
Hello I had a problem with an axis, the control is sinumerik 810D, I replaced the CCU, newest has a version higher and the PLC card is different, I changed the PLC in simatic manager->hardware and I downloaded the program with no problems, but when I try to download the NC the HMI shows 2 alarms 300402 system error in drive link. Error codes 1600,12288 300500 Axis X1 drive 1 system error, error codes 00000002H, 000000CEH ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/28/2016 1:45:21 PMNew subject after splitting |
|
6/28/2016 6:49 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Please provide the complete MLFB number of original & new CCU along with technical details. |
6/29/2016 7:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, CCU3 - 6FC5410-0AY03-0AA1 - PLC 315 -2 DP CCU 3.4 - 6FC5410-0AY03-1AA0 - PLC 314C - 2 DP. Also please check NCU version & s/w details. Please refer below FAQ. Accordingly need software up gradation & then you can re load back up data. SINUMERIK 810D/840D: Supported SFBs/SFCs |
Follow us on