11/29/2019 11:28 AM | |
Joined: 9/9/2014 Last visit: 3/26/2024 Posts: 242 Rating: (40) |
Hello! What order number are the controller? I am sure that first, before updating the software of your controller, you should check why it was not available? What happened to him? And then, when you are convinced that everything is fine with him, update your software))) However, now we have what we have Below is a guide to the controller SIMATIC ET 200SP Open Controller CPU 1515SP PC (F) SIMATIC ET 200SP Open Controller (CPU 1515SP PC) - Current Software Controller versions This is a clipping from the manual. GREEN LED light RED LED off YELLOW LED flashes Maintenance required for the plant. You must exchange the affected hardware within a foreseeable period. Or -------> Firmware update successfully completed ************************* GREEN LED off RED LED off YELLOW LED off i think it's - Starting of the CPU 1515SP PC (F) in the "Windows only" mode Check the system - can you still reach it? ************************* Check that you have done everything according to the instructions Delivery release: SIMATIC S7-1500 Software Controller V2.7 available Try to restore with a flash drive what you have - there are many programs on the Internet how to write an image to a flash drive. 9.4 Restoring delivery state using USB stick (from - Manual, 05/2017, A5E32701806-AC) And I would advise contacting Siemens to send you a backup copy of the disk for your PLC - I'm sure it is possible |
Last edited by: Jen_Moderator at: 11/29/2019 12:03:30Optimized links. Best Regards |
|
This contribution was helpful to1 thankful Users |
Follow us on