8/24/2016 2:43 PM | |
Joined: 2/10/2015 Last visit: 5/16/2024 Posts: 286 Rating: (1) |
hello sir CAOD I have something I do not understand, I wrote a program simatic manager and wanted to integrate WinCC fexible 2008 SP3, but when I right click on the name of my project and then insert a new object I see the other stations (simatic station 300.400, simatic H station, PC simatic station etc ...) but I do not see the Simatic HMI station and same as when I click on insert and then station is also similar and I understand nothing . even when I open WINCC FLEXIBLE and I click on the project, I do not see also integrate an S7 project. I really need your help to solve this problem. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/24/2016 4:18:50 PMNew subject after splitting |
|
8/24/2016 3:20 PM | |
Joined: 9/27/2006 Last visit: 7/31/2024 Posts: 12272 Rating: (2679)
|
Hello frankaay; This document might provide the information you require; How do you integrate a WinCC flexible project in STEP 7? https://support.industry.siemens.com/cs/fr/en/view/38797080 Hope this helps, Daniel Chartier |
8/25/2016 8:43 AM | |
Joined: 7/9/2015 Last visit: 8/1/2024 Posts: 3902 Rating: (574) |
Hi, I think the informations of dchartier are the right ones, but I have got another information / link to this topic How do you restore access to icons and data blocks of STEP 7 from an integrated WinCC flexible project?In this link you will also find a link under further Information to chapter "Integration of WinCC in Step 7" Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on