10/6/2016 10:14 AM | |
Posts: 1 Rating: (0) |
Miss sire. s7-1200 configuration software v10.5 in the configuartion there is a AI card 6ES7-231-4HF 30 OXBO INTHE CONFIGUARTION IT IS MARKT AS S7-1200 SUBSTITUTE DEVICE ITEM.in the device configuration it is markt with a qeustion mark after i installed v12 sp1 the card is not recogniced anymore it flash red led al over the card. upload the program again in v10.5 portal the card is completely disapared. how can i, configer this unknown card again. the program was installed 5 years ago and workt proper untill now. hope to here from you ------------------------------------------------------------------------------------------ Attachmentsiemens.pdf (32 Downloads) |
Last edited by: Min_Moderator at: 10/6/2016 10:37:50 AMNew subject after splitting |
|
10/6/2016 10:22 AM | |
Joined: 5/12/2006 Last visit: 5/2/2024 Posts: 22243 Rating: (2981)
|
Hi, for this module you need a HSP for TIA V10.5 which can be downloaded here: https://support.industry.siemens.com/cs/ww/en/view/40218617 Regards |
Follow us on