10/11/2016 1:43 PM | |
Joined: 10/5/2016 Last visit: 8/18/2021 Posts: 4 Rating: (0) |
Should be fine: SanDisk SDHC 32GB, Class 4 |
10/11/2016 1:59 PM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating: (378)
|
This was my first idea too. If the IOT doesn't boot from SD Card it has no IP address, because the drivers won't be initialized. Maybe a simple reboot (RESET button) helps. You can check if the Ethernet Port of the IOT has a link (the right LED is flashing orange). And make sure to use the X1P1 interface, because only this interface has the IP address 192.168.200.1. The X2P1 IP address is set by DHCP. If there is no link it can be possbile that the IOT didn't boot from SD Card. You can try to wrote the Image to the SD Card again.
You can debug the UART with an adapter cable (TTL-232R-3V3). For example you can use this one. Please give me feedback if one of the steps makes it work! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
10/11/2016 2:42 PM | |
Posts: 15 Rating: (0) |
yes, it is Engineering Sample. Is it normal behaviour then? |
Follow us on