(1)| 10/13/2016 8:37 AM | |
|
Posts: 59 Rating:
|
Hi. I have a problem with uploading a program from the device (CPU 1214C DC/DC/DC) which was created TIA Portal V11 via V12. As it mentioned on forum, it is possible to upload the program by opening "Compatibility Mode V11_V12.ap11" file on V12. And the process should go like a normal uploading. I did it how they said. But unfortunately there's an error message when it would have gone to the end. Could you give some advice with it? Thanks in advance. ------------------------------------------------------------------------------------------ AttachmentV12.zip (466 Downloads) |
Last edited by: Xurshid at: 10/13/2016 8:38:56 AMLast edited by: Min_Moderator at: 10/13/2016 10:02:17 AMNew subject after splitting Last edited by: Min_Moderator at: 10/13/2016 10:07:27 AMAdd links |
|
| 10/13/2016 8:46 AM | |
|
Posts: 59 Rating:
|
By the way, I did it by creating a new empty project, but there's a problem with the compatibility. That's why I opened an existing file ("Compatibility Mode V11_12.ap11"). here's a link: https://support.industry.siemens.com/cs/document/66027369/how-do-you-do-a-program-upload-in-step-7-(tia-portal)-v12-when-the-device-has-been-configured-with-step-7-v11-?dti=0&lc=en-BR |
Last edited by: Xurshid at: 10/13/2016 8:48:03 AM |
|
| 10/13/2016 9:12 AM | |
|
Joined: 5/12/2006 Last visit: 12/19/2025 Posts: 22816 Rating:
|
then create a new empty plc in this project! in you screens you have some Data on the PLC which is overwritten by the upload and this can cause the crash! and don't ocuppy some older topics with the problen, create one topic new for the problem!
|
| 10/13/2016 10:45 AM | |
|
Posts: 59 Rating:
|
Which exactly Data did you mean? I think I haven't add any Data on the PLC, all is put in the file which was I downloaded from this link : https://support.industry.siemens.com/cs/document/66027369/how-do-you-do-a-program-upload-in-step-7-(tia-portal)-v12-when-the-device-has-been-configured-with-step-7-v11-?dti=0&lc=en-BR . I've just opened this file on TIA Portal V12 to upload a program from the device which is on V11, and then added the CPU model on device configuration according to the same device, and connected to the device to be online status. After that, the data would be appeared like on the picture below. At the end, I did upload this from the device. Where did I make a mistake? I can't see it yet. |
Follow us on