(0)| 10/30/2016 7:47 AM | |
|
Posts: 2 Rating:
|
dear all , we face same problem as described above , after changing the CUR board we can not enter the CUR with the parameter controller to change the parameters , not responding on the push-buttons , (and give error code F060) to change the parameters , we need active push-buttons the PMU is normally function on other units new cur card 6SE7090-0XX85-1DA0 Q6T5391565 C98043-A1680-L1 13 old chip was transferred from old cut to new V98113-A1680-A1 4.8 Old CUR card : Q6VN608012 C98043-A1580-L1 15 please advice , we have major equipment down for the moment Thanks up front for your assistance Rene Kwakkel ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/31/2016 2:01:23 PMNew subject after splitting |
|
| 10/31/2016 2:02 PM | |
|
Posts: 4758 Rating:
|
The second thread with the subject After replace Masterdrive fault F060 is located within the conference SIMOVERT MASTERDRIVES. Best regards |
Follow us on