11/4/2016 4:42 PM | |
Joined: 11/28/2015 Last visit: 3/13/2024 Posts: 4 Rating:
|
Hello Daniel, Im having some problems with mapping the slaves using the gateway AC1402 also IFM... maybe can help me. The io address for the AS-i slaves starts at I80 When i set a slave as 1 is everything ok .. i can see the i/os at the right address (I80) no problems, the problem begins when i set as 2 .... i can not see anything .... and when i set as 3 i can see the i/os but at I81 instead of I82... and this continues for any odd address; for example Slave5 appears as I82, slave 7 appears as I83 and etc ... i can not see any even slave at all. There is Swap IO parameter in the Gateway configuration, when i enable it that situation gets inverted... i can not see the odd slaves and i have the mapping io problem with the even slaves. Thanks
------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 11/6/2016 9:23:19 PMNew subject after splitting |
|
Follow us on