11/24/2016 2:48 PM | |
Posts: 3 Rating: (0) |
Hello, I have some question about how to replace SIMODRIVE module. Detail of my drive 1. SIMODRIVE 611 POWER MODULE, Part no. 6SN1123-1AB00-0BA1 version A 2. SIMODRIVE 611-D PLUG-IN UNIT, Part no. 6SN1118-0DH21-0AA1 version C installed in the power module. Now the PLUG-IN unit (2) was fail and I want to replace by the new one which has the same part number, but it has different version. The new one is 6SN1118-0DH21-0AA1 version D. Can I replace the PLUG-IN module version C by version D? If it can be replaced, do I need to do some configuration? or It just OFF and ON, then it can run? Thank in advance. Witthaya AttachmentReplace drive.pdf (456 Downloads) |
Last edited by: k_witt at: 11/24/2016 2:49:59 PM |
|
11/24/2016 11:25 PM | |
Posts: 8 Rating: (0) |
Just insert your good control card. it is 100% sure no different for Ver. C or D. |
This contribution was helpful to1 thankful Users |
11/25/2016 3:58 AM | |
Posts: 3 Rating: (0) |
Thank you very much. |
Follow us on