11/25/2016 9:31 AM | |
Joined: 9/14/2016 Last visit: 1/22/2020 Posts: 59 Rating: (1) |
We have two Scalance X204-2 switches. At first, we connected these switches side by side via 2 m FO cable and it worked. And then, we tried to connect these switches on FO port between two stations the distance is about 250-300 m long. But it wasn't connected. What should we do? Where was the mistake made? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 11/25/2016 2:46:41 PMNew subject after splitting |
|
Follow us on