(0)| 12/8/2016 8:59 PM | |
|
Posts: 8 Rating:
|
Hi APS_84 Recently I bought a 417-5H (6ES7417-5HT06-0AB0) for to replace of my olds CPU 414-4H y 417-4 (this for the recommendation of Siemens). My project has the version 7.1 + SP2 Bundle of PCS7 but does not show me the family 417-5H. Which is the HSP that I need to install to see this family in Hardware Catalog? I hope you can help me, thanks. Attached screenshot. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/12/2016 5:01:31 PMNew subject after splitting |
|
This contribution was helpful to
|
|
| 12/12/2016 5:06 PM | |
|
Posts: 4758 Rating:
|
The second thread with the subject S7 417 5H PLC Compatible With PCS7 V7.1 +SP1 is located within the Process Control Systems SIMATIC PCS 7 conference. Best regards |
Follow us on