12/26/2016 7:20 PM | |
Posts: 1 Rating: (0) |
hello I have a servo amplifier mitsubishi mr-e-70a plug on a plc siemens s7-200 in position mode actuates a servo motor in a cup paper machine and the system works very well. The servo amp is damaged and the cable between that And the plc is grilling. I changed it by another MR-JE-70A and I respect the connection according to the manual but the servo motor does not work. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 12/27/2016 11:45:39 PMNew subject after splitting |
|
5/12/2021 10:18 AM | |
Joined: 4/16/2021 Last visit: 7/15/2024 Posts: 3 Rating: (0) |
Hello AutoGen_919322, Did you finished the project? I need help Siemens plc ve Mitsubishi servo. Kind Regards, Musa UÇAN |
Follow us on