12/28/2016 11:05 AM | |
Joined: 10/30/2012 Last visit: 6/24/2024 Posts: 73 Rating: (1) |
Hello. I am trying to establish UDP connection between 315-2 PN/DP and SCALANCE XR324-12M. I am reffering to this library: Monitoring and Control of Network Components with a SIMATIC S7-PN CPU with the aid of SNMP I am not able to understand how to get the right connection parameters: ipAddress : No problem here. hwIdentifier : What is the hardware identifier? connectionID : What is the connection ID? The example does not have any configured connections. localPort : What is the local port? Why connection in the example is done on different ports?Should I use OpenCommWizard for configuring connection between the CPU and the switch? |
Last edited by: stivanov at: 12/28/2016 11:42:53 AM |
|
Follow us on