(0)| 4/28/2017 10:06 AM | |
|
Joined: 3/2/2007 Last visit: 11/19/2025 Posts: 999 Rating:
|
did the new plc work ok with the tia v13 ? any issues during commissioning ? thank you |
|
... thank you ... |
|
| 4/28/2017 2:15 PM | |
|
Joined: 3/2/2007 Last visit: 11/19/2025 Posts: 999 Rating:
|
any special issues with the modbus rtu rs485 communication ? we are using tia portal v13 sp2 and the plc firmware version is v4.2 thank you 6ES7214-1AG40-0XB0 , SIMATIC S7-1200, CPU 1214C, COMPACT CPU, DC/DC/DC, ONBOARD I/O: 14 DI 24V DC; 10 DO 24 V DC; 2 AI 0 - 10V DC, POWER SUPPLY: DC 20.4 - 28.8 V DC, PROGRAM/DATA MEMORY: 100 KB 6ES7241-1CH30-1XB0 , SIMATIC S7-1200, COMMUNICATION COMMUNICATION BOARD CB 1241, RS485, SCREW CONNECTOR SUPPORTS MESSAGE BASED FREEPORT
|
|
... thank you ... |
|
| 5/22/2017 1:02 PM | |
|
Posts: 58 Rating:
|
Hello, I have configured V4.1 in the hardware config and download it to a V4.2 PLC, but Firmware stays at V4.2. Any help? |
Follow us on