2/17/2017 12:56 PM | |
Joined: 12/3/2016 Last visit: 1/5/2024 Posts: 13 Rating:
|
Hi everyone, I would need Writing and Reading VM in/from Logo8. Here we go: I am using a LOGO8 base device to which I would need to write a value in VM from an CMR2020. They actually both work fine. Unfortunately for design reason I can't use any of the 2 outputs on the CMR2020 since htey they both (#1 and #2) are already configured for another specific purpose. The solution which I am interested would be the following: From the CMR2020 device I would lilke to receive a text message (SMS) which writes a value (e.g. set a blck value to 1) into VM hence triiger an action. Is this something feasible ? Thank you for your help. ------------------------------------------------------------------------------------------ |
Last edited by: tornegeden at: 2/17/2017 12:58:56 PMLast edited by: Min_Moderator at: 2/17/2017 2:23:43 PMNew subject after splitting |
|
2/17/2017 2:07 PM | |
Joined: 12/18/2014 Last visit: 7/3/2024 Posts: 33280 Rating:
|
Take a look at this topic: |
Follow us on