2/20/2017 5:19 PM | |
Joined: 11/21/2011 Last visit: 6/25/2024 Posts: 3 Rating:
|
Portal V14, S7-1500 1515-2 PN CPU, and two CM PtP RS232 HF's as Modbus RTU Slaves. Where do I find the parameters IB_Start / IB_Count / OB_Start / and OB_Count as referred to in the "S7-1500 CM PtP - Configurations for point to point connections" manual (Rev 09/2016) p129 ??? I need to create different PLC I/O areas for each Slave connection in the I/Q areas (NOT Holding register area) which have the same Modbus addresses from the Master point of view. For example: The IB_Start parameter gives me this functionality but the Static area of the IDB created by the Modbus_Slave Block does not show them? I have tried versions V2.2, V2.3 and V2.4. Many thanks in anticipation of your response. posted as new topic "S7-1500 Modbus RTU Slave Address Offsets" ------------------------------------------------------------------------------------------ |
Last edited by: Peter_Apstar at: 2/20/2017 6:11:31 PMLast edited by: Min_Moderator at: 2/21/2017 1:33:12 PMNew subject after splitting |
|
2/21/2017 1:37 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4770 Rating:
|
The second thread with the subject S7-1500 Modbus RTU Slave Address Offsets is published within the conference Communication / Networks. Best regards |
Follow us on