2/24/2017 4:12 PM | |
Posts: 1 Rating: (0) |
Hi all, I have TIA Portal installed in my PC, with STEP 7 v13 and PLCSIM v13 SP1, and in a virtual machine (VMWare) i have my SCADA system in WinCC v7.0. Need to find a way, if it is possible, to connect via TCP/IP (using SIMATIC S7 PROTOCOL SUITE) the Scada and PLCSIM so the tags can be manipulated by the simulated PLC. The link between the Scada and the real PLC is going to be TCP/IP thats why i need to test this configuration. Plus, i have already created all the database with the adresses. Thanks. A.O. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/27/2017 12:02:11 PMNew subject after splitting |
|
Follow us on