(1)| 3/15/2017 10:50 AM | |
|
Posts: 1 Rating:
|
Dear all, i have problem with Sinamic S120 detail : + i use CU320-2DP control 4 encoder motor ( encoder information : PEPPERL + FUCHS, type RHI58N - 0AAK1R61N -01024 ). + Now encoder is brake, i have to changeover control type in Speed Controller from "[21] speed control with Encoder " to "[20] speed control encoderless" of STATER software ( attach image) in oder to system operate continue. + Problem : Current chart is not unsmooth, very rough --> Motor 's gear occur higher vibration than original. + Now, i have to do what ? Looking forward your help? Thanks !!! ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 3/16/2017 11:08:44 AMNew subject after splitting |
|
| 3/16/2017 5:18 PM | |
|
Joined: 10/11/2006 Last visit: 1/23/2026 Posts: 6074 Rating:
|
Hello +84989056958, In closed loop speed control without encoder, it is not possible, reaching the same dynamics as with encoder. E.g. If it doesn't succeed : 2nd step: p1470 from 6.326 to 4 and p1472 from 75.6 to 130ms |
|
With best regards, |
|
| 7/10/2017 2:43 PM | |
|
Posts: 8171 Rating:
|
New question published by ismail_ is split to a separate thread with the subject Is it possible to give tolerans or time delay at the Sinamics s120 parameter?. Best regards |
Follow us on