7/17/2017 2:14 PM | |
Posts: 6 Rating: (0) |
Hi HMK, could you please tell me, beyond the npm packages below, do you remember what npm packages you installed on IOT2000? -azure-iot-device -azure-iot-device-mqtt -azure-iot-device-http -azure-iot-device-amqp I have some issues (pictures attached) to estabilish the connection between the Azure IOT hub and the IOT2000. When I send a message to the IOT Hub node in node-red, it shows the follow message: "Error while trying to send message:Error: AMQP Transport: Could not connect"
AttachmentScreenshots.zip (561 Downloads) |
7/18/2017 12:01 PM | |
Joined: 3/17/2014 Last visit: 1/15/2024 Posts: 53 Rating: (12) |
Hi, I post a complete guide for IOT Connection to Azure using node-red-contrib-azureiothubnode. Hope can it helps. AttachmentIOT2040_Azure_Connection_eng.pdf (1082 Downloads) |
This contribution was helpful to6 thankful Users |
3/17/2019 8:13 PM | |
Joined: 8/13/2016 Last visit: 4/21/2024 Posts: 55 Rating: (2) |
Yep, I too am looking for some guidance... If anyone can help. I can follow the old guide up to the point where you try to login (Step 2!) Then get an error that this is an unknown command. Fiddled about trying to get the CLI installed but having a nightmare.
|
5/24/2019 3:11 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, For me it fails to install over script or pip3. Still trying to figure out a workaround... Kind regards! |
Follow us on