4/1/2017 11:03 AM | |
Joined: 10/11/2016 Last visit: 6/19/2024 Posts: 6 Rating:
|
Hi, Can anyone tell me that when CPU 315-2 DP already running and I'm downloading modbus Slave Drivers to CP341. Is that CPU will go to Stop Mode or not. Actually Plant is Running and I am doing working on it. Please Guide. Thanks in Advance. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/3/2017 4:07:30 PMNew subject after splitting |
|
4/1/2017 3:03 PM | |
Joined: 9/9/2015 Last visit: 6/24/2024 Posts: 727 Rating:
|
to load driver into the device, the CPU is required to stop. If not, you will get a dialog box which disallow you from downloading the driver. But you can actually load the driver by using other CPUs then insert it back to the running one. This works in my previous project. We load the driver first in the office and bring it to site. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to
1 thankful Users |
Follow us on