4/7/2017 6:28 PM | |
Joined: 1/26/2007 Last visit: 5/2/2024 Posts: 123 Rating: (4) |
Hello , I have the same issue. i am using an Im151-8PN and in configuration at some point i have an module 4Ai TC ST 6ES7 134 -4JD00- 0AB0. I am using an termocuple Type K and instead of actual value( about 10 o C) i get aproximately - 10oC . Haw i can solve the issue ? I do not want to use offset for cerrecting this. Is teher any solution for this ? I mention i have send back first termocuple type K cause i thought it is deffect. Now i have received another brand new , and the same situation. Thank you a lot for your response ------------------------------------------------------------------------------------------ |
Last edited by: aliuta2000 at: 4/7/2017 6:30:50 PMLast edited by: Min_Moderator at: 4/10/2017 3:41:48 PMNew subject after splitting |
|
4/12/2017 9:37 PM | |
Joined: 9/23/2005 Last visit: 5/10/2024 Posts: 4529 Rating: (699) |
Please RTFM.
The question is what this voltage represents.
I didn't say this. But this can be also an option. The contributors to this Forum are volunteers. If it's so urgent pls contact Siemens Support directly or hire someone who knows what to do. |
Regards, |
|
Follow us on