5/2/2017 7:53 AM | |
Posts: 3 Rating: (0) |
Hello. Tried to install v14 now many times without sucsess. Tried to install all the new windows updates. Every time it's getting "installed", but its not possible to start it up. A error message is occuring after installation. (se log file). I had V12 before and that was working ok. Tried to follow some things from the forum like to uninstall, remove directory after uninstall and also remove files from the registry. Anyone? Pc spec: WIN7, 64bit, intel i7. AttachmentSIA_STEP7_BASIC_V14@17-05-02_07-30-24_summary - logfile.txt (1022 Downloads) |
Last edited by: kim.milde at: 5/8/2017 6:52:22 AMLast edited by: Jen_Moderator at: 9/3/2018 7:01:55 AM |
|
5/2/2017 9:57 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi kim, What try to install the TIA V14 Trial incl SP1. You can download it here: SIMATIC STEP 7 including PLCSIM V14 SP1 TRIAL download hope this helps, regards, |
FCK WAR! |
|
5/3/2017 12:48 PM | |
Posts: 3 Rating: (0) |
SP1 did not work either. Failed at the same point. See attachment
AttachmentSIA_STEP7_BASIC_V14_SP1@17-05-03_10-50-06_summary logfile.txt (548 Downloads) |
5/3/2017 1:14 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1054) |
hi kim.milde, try to deinstall everything with the instructions from this FAQ: How do you uninstall STEP 7 (TIA Portal) completely? Then install the Trial, I posted before. Do the installation with deactivated anti-virus-scan and with full admin-rigths(rigth-click on setup.exe -> run as admin) hope this helps, regards, |
FCK WAR! |
|
11/4/2017 9:15 AM | |
Posts: 1 Rating: (0) |
Hello I have same problem I have tried to install new TiaPortal V14 without any success. Disabled antivirus, started installation with full right.... unfortunately nothing didn't work. Any idea how to fix it ? AttachmentSIA_STEP7_BASIC_V14_SP1@17-11-04_08-43-42_summary.docx (441 Downloads) |
This contribution was helpful to1 thankful Users |
9/3/2018 7:00 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
New question published by jirieibel.innofreight is split to a separate thread with the subject TIA Portal v15 on win7 fails during installation. Best regards |
Follow us on