5/31/2017 2:58 PM | |
Joined: 8/25/2006 Last visit: 8/14/2024 Posts: 2208 Rating: (278)
|
1. @CTV, connector AT: T1 - channel name, 3 - slave address, 0 - byte order. 2. You should create virtual connections at block outputs with the name used at connector CRT of @CTV, i.e '!T1' and a number. 3. There is a SW ComProfibus, that is used for configuring slaves of SS52 using their gsd-files. |
This contribution was helpful to1 thankful Users |
7/25/2017 11:57 AM | |
Posts: 17 Rating: (0) |
I still have a problem creating a communication between Simadyn and a Profibus slave ( dSPACE card DS4502) Even though the I/O Mapping of the slave (program Sycon from Hilscher) and the Simadyn (COMProfibus) looks the same, the diagnostic of COMProfibus says that the bus configuration between master and slave is different. I upload some screenshots hoping someone can point out possible corrections to do. thank you very much! ---- UPDATE ------- Solved, be really careful in the I/O Mapping distinguishing byte/word... and byte/word CON: are different type of data for the slots! AttachmentCOMprofibus on PG + mapping slave.zip (406 Downloads) |
Last edited by: guerrez at: 7/25/2017 3:41:41 PM |
|
9/1/2017 1:02 PM | |
Joined: 8/21/2014 Last visit: 8/14/2024 Posts: 1006 Rating: (13) |
New question published by Pawant02 is split to a separate thread with the subject I have a s5 135u and a simadyn d. They both look healthy but i cannot get communication between them. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on