6/5/2017 5:17 PM | |
Joined: 12/10/2011 Last visit: 7/25/2024 Posts: 39 Rating:
|
Dear all, even if the topic is old I'd like to use it in order to understand an error message when I try to connect with UA server. I'm receiving the error "An error occurred while searching for endpoints. Object reference not set to an instance of an object". Has somebody any idea, please? I care to underline that I could connect and communicate with the PLC (PLC sim 1500) in other VM by other OPC client, but I couldn't do it with OPC Scout 10. Thanks in advance. Max ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/9/2017 3:32:47 PMNew subject after splitting |
|
4/5/2019 3:57 PM | |
Posts: 3 Rating:
|
Hello, This problem is resolved by enable/tick mark the option "use as target for symbol download". |
This contribution was helpful to
1 thankful Users |
9/27/2021 9:45 AM | |
Joined: 8/3/2009 Last visit: 7/25/2024 Posts: 13373 Rating:
|
Hello leafgreen1 Please give us some more Information: - Which TIA Portal Version do you use? - Which S1500 and FW Version do you use? - Check the FAQs if you have done all nessesary steps: https://support.industry.siemens.com/cs/de/en/view/109737901 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on