6/24/2017 1:44 PM | |
Joined: 4/18/2014 Last visit: 10/4/2024 Posts: 253 Rating: (5) |
Mr.IBN, Please check my first post , This is the new CPU (314C-2DP) and i not yet programmed just i am monitoring the Input address in OB1 with one NO and Coil find the attached program back up. And also if it is an hardware problem then is it possible that the same issue will happen for both old and new CPU. And if it is program Error kindly check the attached back up. Thanks for your advice i stopped crying. AttachmentTest.zip (342 Downloads) |
Follow us on