7/12/2017 12:46 PM | |
Posts: 74 Rating: (1) |
Hello all, Are there anybody that could share an VC++ example with me that read/write a tag from WinCC? I can not get it to work. Cheers Raffe |
7/12/2017 1:00 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2164)
|
Hello Raffepersson1, with ODK the tags are read with the function "DMGetValue", and written with the function "DMSetValue", some examples are in the ODK-documentation. Regards Georg Berghof AttachmentODK_DM_GET_SET_Value.txt (153 Downloads) |
PS: If this post did really help you, you may use the Rate-button |
|
7/12/2017 1:30 PM | |
Posts: 74 Rating: (1) |
Thanks Georg for the answer. I can not find any VC++ example that works? I got ODK 7.3. Can you share an VC++ project with me? Raffe |
7/14/2017 9:15 AM | |
Posts: 74 Rating: (1) |
Thanks Georg. Anybody that can help me? |
Follow us on