7/20/2017 8:22 AM | |
Joined: 4/8/2016 Last visit: 2/13/2024 Posts: 133 Rating: (45) |
Hello niksss, I cannot give you a detailed answer for your requirements, but here some thoughts that might help: 1. For new PCS 7 plants it is recommended to use the CPU 410-5H Process Automation. You can use two of this CPU in a redundant automation system and it is suitable for fail-safe applications. You can find more information in the Industry Mall:https://mall.industry.siemens.com/mall/en/WW/Catalog/Products/9990067?tree=CatalogTree 2. For Failsafe IO in PCS 7 you can use the ET 200M. The ET 200M supports redundant communication with the PROFIBUS Interface Modules. IO redundancy is supported with MTA and Power Supplies. More information in the Industry Mall: 4. For both CPU and ET 200M are Power Supplies for 110V AC available. 5. The latest PCS 7 Version is V9.0 and for the failsafe logic you need F Systems. More information in the Industry Mall: |
Last edited by: 51N3P at: 7/20/2017 9:08:06 AMKind regards |
|
This contribution was helpful to1 thankful Users |
7/20/2017 8:33 AM | |
Posts: 57 Rating: (0) |
Thank you 51n3p |
4/9/2018 8:11 AM | |
Joined: 6/19/2017 Last visit: 5/7/2024 Posts: 8002 Rating: (163) |
New question published by Ashwin29 is split to a separate thread with the subject What is Basic Difference between Normal PLC and Safety plc?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on