4/25/2008 5:30 AM | |
Posts: 2661 Rating: (279) |
Amit: Can you please explain your problem a bit more clearly? From what I could gather from your description, you are not able to see the START nub in SFC external view? I tried on my V7.0 SP1 and I can see the START. See attachment. Regards, Phantom AttachmentDokument1.pdf (326 Downloads) |
4/25/2008 4:18 PM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Dear Phantom75 plz find the attached BMP file for SFC external view for my connection. in that same signal interconnection done for abort which is given to start but on abort it wasNOT connected. Start signal was 0 & Abort was 1 but the that day my SFC show me the Running also the Run (in SFC external view) show me 1 that time. so tell me due to which reson it will show me in run mode. |
Ammy |
|
5/1/2008 11:32 PM | |
Posts: 2661 Rating: (279) |
Amit: AttachmentDokument1.pdf (394 Downloads) |
5/3/2008 8:41 AM | |
Joined: 4/19/2008 Last visit: 6/25/2024 Posts: 1525 Rating: (159) |
Dear Phantom75, I made ENMAN connection as you shown in Attachment. & rests of the connection aresame as pervious.Still we are not overcome in problem. Then Abort command is 1 Start is 0, and then also SFC shows the Run condition. I observed that when my SFC is HOLD & not resume for long time that time such problem occurred, after this problem If I stop the SFC & start & again Stop it the it shows me Abort . If I will Get the Snap SFC of same I will attached same. Amit |
Ammy |
|
5/3/2008 9:15 AM | |
Posts: 2661 Rating: (279) |
Amit: Is it possible for you to post your project (or PM) so that I can try on my machine? Regards |
Follow us on