8/24/2017 3:56 PM | |
Posts: 9 Rating:
|
Hello dears experts: I have the follow problem with the analog input read, I need to change a pressure sensor, the original sensor is 0...6 mbars with an output 4...20 mA and I have a newone 0....16 mbars with an output 4...20 mA. I try all the optios in the manual of CPU 115 for the FB250 without succes (see the atachment FB250.jpg). The problem is that the scaling is on UGR: + 0 and OGR: + 29000 originally and If I change the OGR to + 32767, the value of the process tha i need to adjust dosent all . I dont want tho change the program of the PLC because i dont have the original code, and i thinhk is not nesesary. The configuration block that I have is on the FB250_program_block.jpg. Thanks for your apriciated support ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 8/25/2017 8:04:44 AMNew subject after splitting |
|
This contribution was helpful to
1 thankful Users |
8/24/2017 3:58 PM | |
Posts: 9 Rating:
|
This is the program code on the CPU ( see the atachmen) |
8/25/2017 8:05 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8192 Rating:
|
|
My Forum is the place to personalize your profile, |
|
Follow us on