8/29/2017 9:37 AM | |
Joined: 8/15/2015 Last visit: 3/14/2024 Posts: 72 Rating: (7) |
Can someone help me with a corrupt project file please? Im trying to understand what the logic is behind the system deciding to save it as a modus project? normally it is saved as .LSC , but this is saved as .MNP.... A possible issue is that I'm recycling a project written for an FS03 unit, written using Comfort Soft 8.0 This was a Stand alone LOGO 12/24 - FS03 - mid 2016 Current setup is a LOGO 12/24 FS04 with three other units sharing network inputs and outputs. I wrote the whole program, tested by simulation, loaded project onto main unit and one of the other feeder units. all fine.. Then i wanted to change something, offline. i open the project, and as soon as i click on any unit, it does the "loading' dialogue repeatedly and the task has to be killed ... any one willing to take a look? I'd prefer not to post it open to the forum. Thanks ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 8/29/2017 10:43:51 AMNew subject after splitting The more mistakes I make, the faster I learn! |
|
8/29/2017 9:57 AM | |
Joined: 12/18/2014 Last visit: 5/7/2024 Posts: 32988 Rating: (4076)
|
When you not will to upload in the forum, then send it me per PN. |
8/31/2017 11:08 AM | |
Joined: 8/15/2015 Last visit: 3/14/2024 Posts: 72 Rating: (7) |
Hi This seems to be something else, not the project. I was able to rebuild the whole project and load it into the modules. The program was completely faulty on modules values did not apply to some blocks and other set values were counting up when they were static.... corrupt.. so I reverted to a working (basic) version and decided to try again two days later. Now the project refuses to open fully, on the same desktop PC I wrote this on. (opens to see the list on the left, then as soon as a diagram is selected ..... cycles the 'loading' dialogue box. The project is saved on my One Drive. It refuses to load on my Laptop too. Has it got to do with the multiple connections between modules and I've made a mistake? It might be too many...? Or is it because I closed LSC and Java freaked out? Frustrated AttachmentKatkop Sluice System progress with errors.zip (171 Downloads) |
The more mistakes I make, the faster I learn! |
|
Follow us on