9/4/2017 6:09 AM | |
Joined: 1/27/2012 Last visit: 6/20/2024 Posts: 84 Rating: (1) |
Hello, After so many years, the problem is still there. I am using PLCSIM V5.4 SP5 Upd2. I can not access the IOs that are configured in Profinet IO system. I was in impression that I did something wrong. But now i know it is not working with PLCSIM. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/4/2017 9:07:56 AMNew subject after splitting |
|
This contribution was helpful to2 thankful Users |
Follow us on