9/6/2017 5:51 PM | |
Posts: 5 Rating: (0) |
Hi Miami, Could you please give me a code demo using this way to control servo motor? "You will have to fill the encoder and drive status in the "Input" section of the DB in the OB PreServo. And use the "output" section of the DB in the OB PostServo." I try to find a document to follow as you said. But I can't. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 9/8/2017 9:53:44 AMNew subject after splitting |
|
9/6/2017 6:55 PM | |
Joined: 8/31/2005 Last visit: 6/14/2024 Posts: 2198 Rating: (328) |
The TO is expecting a drive following the PROFIdrive profile. When you set the Bits "out2" and "out3" in the control word the drive will set correspondending bits in the statusword. If you have no drive following the PROFIdrive profile, you have to simulate it. I haven't programmed it, so I can't present a "drive simulation" code. Have a look on the status and control word (see attachment, row "comments").
AttachmentCTW-STW.pdf (404 Downloads) |
|
|
9/8/2017 9:21 AM | |
Posts: 5 Rating: (0) |
Hi, Miami. Thank you for your reply. I want to add more questions. Can we use Motion Control Datablock Encoder to control MINAS A6 servo drives? Thanks.
|
9/8/2017 9:27 AM | |
Joined: 5/12/2006 Last visit: 7/17/2024 Posts: 22317 Rating: (2998)
|
Hi, i think not. For that the PROFIDRIVE is not specified so the TO objects can't work with it. Regards Christoph |
9/8/2017 10:29 AM | |
Posts: 5 Rating: (0) |
Hi, Christoph. Thank you for your reply. Can you list all devices like MINAS A6 servo drives that supported PROFIDRIVE? Regards Quinn |
9/8/2017 10:37 AM | |
Joined: 5/12/2006 Last visit: 7/17/2024 Posts: 22317 Rating: (2998)
|
Hi, sorry i don't know such a list. |
Follow us on