9/12/2017 9:39 PM | |
Posts: 1 Rating: (0) |
hi I have a problem with aSimodrive 6SN1118-0NK01-0AA1. I have an error code: E-A597. could you help me? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/13/2017 2:05:36 PMNew subject after splitting |
|
9/14/2017 10:25 AM | |
Joined: 10/17/2007 Last visit: 6/26/2024 Posts: 4007 Rating: (350) |
A597 is error 597 PROFIBUS: Drive not in synchronism. Supplementary information: \%X Cause Supplementary information 0x01: The master sign-of-life (STW2, bits 12--15) has more consecutive failures than permitted. The permissible sign-of-life error is specified using P0879 bit 2--0 (PROFIBUS configuration). 0x02: The Global Control telegram to synchronize the clock cycles has failed in operation for several DP cycles in a row or has violated the time grid (refer to times Tdp and Tpllw) -- specified using the parameterizing telegram -- for several DP clock cycles in a row. If the complete DP communications fails permanently, then Fault 599 is also output -- at the latest after the response monitoring time specified when the bus was configured, expires. Remedy -- Check whether communications is briefly or continuously interrupted. -- Check whether the PROFIBUS master can operate in clock cycle synchronism and the Global Control Telegrams, required for clock cycle synchronous operation, are output in the equidistant DP clock cycle. -- Check whether clock synchronism has been activated in the bus configuration, although it is not controlled by the master used. -- Check whether the master sign-of-life (STW2, bits 12--15) is received and is incremented in the parameterized clock cycle. Acknowledgement RESET FAULT MEMORY
|
If you like my comments please |
|
Follow us on