9/7/2017 4:01 PM | |
Posts: 11 Rating: (0) |
Hi, i'm trying to use Openess with a sample project with Tia Porta v.14. When i try to run some snippet of code with break points, i show an error message in visual studio: “The function evaluation requires all threads to run”This error message is in visual studio 2017. I've installed visual studio 2015 but the message compare again. Is a problem becouse i can't navigate inside object/items I do not think it's a visual studio configuration problem because it is only with Openess libraries that causes these problems. Thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 9/19/2017 2:05:09 PMNew subject after splitting |
|
9/22/2017 10:33 AM | |
Joined: 1/4/2010 Last visit: 9/25/2024 Posts: 650 Rating: (40) |
Hi, https://support.industry.siemens.com/cs/ww/de/view/109251656/en?dl=en in the part: I hope this is helpful for you. Kind Regards |
Regards |
|
Follow us on